REGEN.POWERFILTERED

Description

This parameter returns a filtered value of REGEN.POWER. A single order lowpass of 1/REGEN.TEXT Hz is applied to generate REGEN.POWERFILTERED.

If REGEN.POWERFILTERED exceeds the value of REGEN.WATTEXT, Fault 2010 (Regen overpower) will be generated.

This keyword may be recorded in the scope screen for analysis.

Example

REGEN.TEXT = 10 (seconds)

Lowpass Filter Frequence = 1/10 seconds = 0.1 Hz

REGEN.POWERFILTERED = REGEN.POWER * 0.1Hz lowpass

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

Watt

Range

0 to REGEN.WATTEXT

Default Value

N/A

Data Type

Integer

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

REGEN.POWERFILTERED

3007h

01h

Unsigned32

-

-

Read only

Yes

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

2405

1

2405 (0x965)

REGEN.POWERFILTERED

Unsigned32

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

REGEN.POWERFILTERED

2405

Unsigned32

Read Only

-